Clean and highly efficient, ABB’s new SureWave Static Frequency Converter ensures the static, seamless, and automated transfer of power from a ship’s onboard generator to an onshore power source, removing the need to use diesel burning generators when in port.
Switching to this next generation of static conversion technology will enable ship owners to avoid fines and taxes imposed for not using shore power once berthed.
ABB has engineered SureWave SFC to be 50 percent smaller than previous models and for added flexibility, it can be installed on the marine vessel or port side. To further increase energy efficiency and reduce carbon emissions, ABB’s SureWave can be paralleled or connected to renewable energy sources like PV or wind farms. As frequency and voltage can vary between ports around the world, SureWave SFC allows more flexibility when connecting 60 Hz powered equipment to a 50 Hz supply network or 50 Hz powered equipment to a 60 Hz supply network