The global mining industry must navigate a multitude of megatrends. Minerals and metals are essential in the transition towards net zero as clean energy technologies typically require more significant quantities of minerals than fuel-based solutions. Another trend is rapid urbanization, which drives enormous investments in infrastructure and construction projects that depend heavily on materials procured through mining. Therefore, it’s important to reduce the carbon and environmental cost of obtaining them.
The mining industry needs to take steps to improve energy efficiency, productivity, and reduce emissions. One crucial area to focus on is the grinding mill, as this equipment has the most significant impact on the performance and sustainability of mining operations and is responsible for up to 40% of a mining facility’s total energy usage.
Utilizing well-established technology, such as variable speed drives (VSDs) paired with high-efficiency electric motors, can optimize productivity, and ensure availability while reducing energy consumption.